AXIS#.HOME.MOVE

Description

AXIS#.HOME.MOVE starts a homing move. AXIS#.OPMODE must be set to 2 (position mode) and AXIS#.CMDSOURCE must be set to 0 (Service).

AXIS#.STOP can be used to stop homing after it has started.


  • When Axis 2 is configured as a gantry (AXIS2.CMDSOURCE = 4), issuing AXIS1.HOME.MOVE starts homing on both Axis 1 and Axis 2. The drive returns an error if AXIS2.HOME.MOVE is commanded.
    To ensure both axes move together during gantry homing, AXIS1.HOME.V, AXIS1.HOME.ACC. and AXIS1.HOME.DEC are used on both axes. The correspoding AXIS2 parameters are ignored.
    When homing completes successfully on both axes, GANTRY.STATE changes to 3, indicating the gantry is active and ready for motion commands.

Versions

Action Version Notes
Implemented 02-00-00-000
Modified 02-05-00-000 Added gantry homing support

General Information

Type

Command

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

See Also

AXIS#.HOME.MODE

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6108

1

6108 (0x17dc)

AXIS1.HOME.MOVE

Unsigned8

Read/Write

No

71644

2

6108 (0x17dc)

AXIS2.HOME.MOVE

Unsigned8

Read/Write

No

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.HOME.MOVE

6108

Unsigned8

Read/Write

-

Related Topics

Homing

Gantry Mode